AXIS#.PL.INTINMAX
Description
AXIS#.PL.INTINMAX limits the input of the position loop integrator by setting the input saturation. When used in concert with AXIS#.PL.INSATOUT, this variable allows you to make the position loop integrator effective near the target position. Far from the target position, however,the integrator is not dominant in the loop dynamics.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
N/A |
|
Data Type |
Float |
|
See Also |
AXIS#.PL.FB |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Related Topics
AXIS#.PL.ERR | AXIS#.PL.ERRFTHRESH | | AXIS#.PL.ERRWTHRESH | Position Loop